3.4.4.29 USB_HOST_CDC_RESULT Enumeration
C
typedef enum {
USB_HOST_CDC_RESULT_FAILURE,
USB_HOST_CDC_RESULT_BUSY,
USB_HOST_CDC_RESULT_REQUEST_STALLED,
USB_HOST_CDC_RESULT_INVALID_PARAMETER,
USB_HOST_CDC_RESULT_DEVICE_UNKNOWN,
USB_HOST_CDC_RESULT_ABORTED,
USB_HOST_CDC_RESULT_HANDLE_INVALID,
USB_HOST_CDC_RESULT_SUCCESS
} USB_HOST_CDC_RESULT;
Summary
USB Host CDC Client Driver Result.
This enumeration lists the possible results the CDC client driver uses. Only some results are applicable to some functions and events. Refer to the event and function documentation for more details.
Members
| Members | Description |
| USB_HOST_CDC_RESULT_FAILURE | An unknown failure has occurred |
| USB_HOST_CDC_RESULT_BUSY | The transfer or request could not be scheduled because internal queues are full. The request or transfer should be retried |
| USB_HOST_CDC_RESULT_REQUEST_STALLED | The request was stalled |
| USB_HOST_CDC_RESULT_INVALID_PARAMETER | A required parameter was invalid |
| USB_HOST_CDC_RESULT_DEVICE_UNKNOWN | The associated device does not exist in the system. |
| USB_HOST_CDC_RESULT_ABORTED | The transfer or requested was aborted |
| USB_HOST_CDC_RESULT_HANDLE_INVALID | The specified handle is not valid |
| USB_HOST_CDC_RESULT_SUCCESS | The operation was successful |
Remarks
None.