3.4.4.8 USB_HOST_CDC_SerialStateNotificationGet Function
C
USB_HOST_CDC_RESULT USB_HOST_CDC_SerialStateNotificationGet(
USB_HOST_CDC_HANDLE handle,
USB_HOST_CDC_TRANSFER_HANDLE * transferHandle,
USB_CDC_SERIAL_STATE * serialState
);
Summary
This function will request Serial State Notification from the attached device. If the request was accepted, transferHandle will contain a valid transfer handle, else it will contain USB_HOST_CDC_TRANSFER_HANDLE_INVALID. The completion of the request will be indicated by the USB_HOST_CDC_EVENT_SERIAL_STATE_NOTIFICATION_RECEIVED event. The transfer handle will be returned in the event.
Precondition
The client handle should be valid.
Parameters
| Parameters | Description |
| handle | handle to the CDC device instance to which the request should be sent. |
| transferHandle | Pointer to USB_HOST_CDC_TRANSFER_HANDLE type of a variable. This will contain a valid transfer handle if the request was successful. |
| serialState | Pointer to the serial state data structure where the received serial state will be stored. |
Returns
USB_HOST_CDC_RESULT_SUCCESS - The operation was successful.
USB_HOST_CDC_RESULT_DEVICE_UNKNOWN - The device that this request was targeted to does not exist in the system.
USB_HOST_CDC_RESULT_BUSY - The request could not be scheduled at this time. The client should try again.
USB_HOST_CDC_RESULT_INVALID_PARAMETER - An input parameter was NULL.
USB_HOST_CDC_RESULT_FAILURE - An unknown failure occurred.
USB_HOST_CDC_RESULT_HANDLE_INVALID - The client handle is not valid.
Remarks
None.