3.4.4.3 USB_HOST_CDC_AttachEventHandlerSet Function
C
USB_HOST_CDC_RESULT USB_HOST_CDC_AttachEventHandlerSet(
USB_HOST_CDC_ATTACH_EVENT_HANDLER eventHandler,
uintptr_t context
);
Summary
This function will set an attach event handler. The attach event handler will be called when a CDC device has been attached. The context will be returned in the event handler. This function should be called before the bus has been enabled.
Precondition
None.
Parameters
| Parameters | Description |
| eventHandler | pointer to the attach event handler. |
| context | an application defined context that will be returned in the event handler. |
Returns
USB_HOST_CDC_RESULT_SUCCESS - if the attach event handler was registered successfully.
USB_HOST_CDC_RESULT_FAILURE - if the number of registered event handlers has exceeded USB_HOST_CDC_ATTACH_LISTENERS_NUMBER.
Remarks
Function should be called before USB_HOST_BusEnable() function is called.