Mapping of the write strobe signal WSTRB to write data WDATA is done on a
phased basis, by mapping WDATA to the QDR data bus D, as shown in Figure 5-10 and Figure 5-11. However, it is also aligned to BWSx_N signals on the QDR interface as
follows. Note that the following example is for SRAM_DWIDTH of 36, or x36 mode.
Table 5-4. WSTRB to BWS Mapping| WSTRB Index | BWS Index |
|---|
| 7:0 | 0 |
| 15:8 | 1 |
| 23:16 | 2 |
| 31:24 | 3 |
Within each WSTRB byte, each bit corresponds to a clock cycle (phase) and either rising or falling edge. A complete mapping for write data bus WDATA to WSTRB is listed in the following tables, for x36, x18, and x9 modes.
Table 5-5. Write Data to Write Strobe Mapping (x36)| WSTRB_MAPPING_INDEX | WDATA INDEX | RISING/FALLING | CLOCK CYCLE |
|---|
| 0 | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | RISING | 1 |
| 8 | 36 | 37 | 38 | 39 | 40 | 41 | 42 | 43 | 44 | FALLING | 1 |
| 16 | 72 | 73 | 74 | 75 | 76 | 77 | 78 | 79 | 80 | RISING | 2 |
| 24 | 108 | 109 | 110 | 111 | 112 | 113 | 114 | 115 | 116 | FALLING | 2 |
| 1 | 144 | 145 | 146 | 147 | 148 | 149 | 150 | 151 | 152 | RISING | 3 |
| 9 | 180 | 181 | 182 | 183 | 184 | 185 | 186 | 187 | 188 | FALLING | 3 |
| 17 | 216 | 217 | 218 | 219 | 220 | 221 | 222 | 223 | 224 | RISING | 4 |
| 25 | 252 | 253 | 254 | 255 | 256 | 257 | 258 | 259 | 260 | FALLING | 4 |
| 2 | 9 | 10 | 11 | 12 | 13 | 14 | 15 | 16 | 17 | RISING | 1 |
| 10 | 45 | 46 | 47 | 48 | 49 | 50 | 51 | 52 | 53 | FALLING | 1 |
| 18 | 81 | 82 | 83 | 84 | 85 | 86 | 87 | 88 | 89 | RISING | 2 |
| 26 | 117 | 118 | 119 | 120 | 121 | 122 | 123 | 124 | 125 | FALLING | 2 |
| 3 | 153 | 154 | 155 | 156 | 157 | 158 | 159 | 160 | 161 | RISING | 3 |
| 11 | 189 | 190 | 191 | 192 | 193 | 194 | 195 | 196 | 197 | FALLING | 3 |
| 19 | 225 | 226 | 227 | 228 | 229 | 230 | 231 | 232 | 233 | RISING | 4 |
| 27 | 261 | 262 | 263 | 264 | 265 | 266 | 267 | 268 | 269 | FALLING | 4 |
| 4 | 18 | 19 | 20 | 21 | 22 | 23 | 24 | 25 | 26 | RISING | 1 |
| 12 | 54 | 55 | 56 | 57 | 58 | 59 | 60 | 61 | 62 | FALLING | 1 |
| 20 | 90 | 91 | 92 | 93 | 94 | 95 | 96 | 97 | 98 | RISING | 2 |
| 28 | 126 | 127 | 128 | 129 | 130 | 131 | 132 | 133 | 134 | FALLING | 2 |
| 5 | 162 | 163 | 164 | 165 | 166 | 167 | 168 | 169 | 170 | RISING | 3 |
| 13 | 198 | 199 | 200 | 201 | 202 | 203 | 204 | 205 | 206 | FALLING | 3 |
| 21 | 234 | 235 | 236 | 237 | 238 | 239 | 240 | 241 | 242 | RISING | 4 |
| 29 | 270 | 271 | 272 | 273 | 274 | 275 | 276 | 277 | 278 | FALLING | 4 |
| 6 | 27 | 28 | 29 | 30 | 31 | 32 | 33 | 34 | 35 | RISING | 1 |
| 14 | 63 | 64 | 65 | 66 | 67 | 68 | 69 | 70 | 71 | FALLING | 1 |
| 22 | 99 | 100 | 101 | 102 | 103 | 104 | 105 | 106 | 107 | RISING | 2 |
| 30 | 135 | 136 | 137 | 138 | 139 | 140 | 141 | 142 | 143 | FALLING | 2 |
| 7 | 171 | 172 | 173 | 174 | 175 | 176 | 177 | 178 | 179 | RISING | 3 |
| 15 | 207 | 208 | 209 | 210 | 211 | 212 | 213 | 214 | 215 | FALLING | 3 |
| 23 | 243 | 244 | 245 | 246 | 247 | 248 | 249 | 250 | 251 | RISING | 4 |
| 31 | 279 | 280 | 281 | 282 | 283 | 284 | 285 | 286 | 287 | FALLING | 4 |
| (1) The mapping
is not sequential. First bit of write_strobe corresponds to the first 9 wdata
bits. The second bit does not correspond to the next 9 wdata bits. | |
Table 5-6. Write Data to Write Strobe Mapping (x18)| WSTRB_MAPPING_INDEX | WDATA INDEX | RISING/FALLING | CLOCK CYCLE |
|---|
| 0 | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | RISING | 1 |
| 8 | 36 | 37 | 38 | 39 | 40 | 41 | 42 | 43 | 44 | FALLING | 1 |
| 1 | 72 | 73 | 74 | 75 | 76 | 77 | 78 | 79 | 80 | RISING | 2 |
| 9 | 108 | 109 | 110 | 111 | 112 | 113 | 114 | 115 | 116 | FALLING | 2 |
| 2 | 9 | 10 | 11 | 12 | 13 | 14 | 15 | 16 | 17 | RISING | 3 |
| 10 | 45 | 46 | 47 | 48 | 49 | 50 | 51 | 52 | 53 | FALLING | 3 |
| 3 | 81 | 82 | 83 | 84 | 85 | 86 | 87 | 88 | 89 | RISING | 4 |
| 11 | 117 | 118 | 119 | 120 | 121 | 122 | 123 | 124 | 125 | FALLING | 4 |
| 4 | 18 | 19 | 20 | 21 | 22 | 23 | 24 | 25 | 26 | RISING | 1 |
| 12 | 54 | 55 | 56 | 57 | 58 | 59 | 60 | 61 | 62 | FALLING | 1 |
| 5 | 90 | 91 | 92 | 93 | 94 | 95 | 96 | 97 | 98 | RISING | 2 |
| 13 | 126 | 127 | 128 | 129 | 130 | 131 | 132 | 133 | 134 | FALLING | 2 |
| 6 | 27 | 28 | 29 | 30 | 31 | 32 | 33 | 34 | 35 | RISING | 3 |
| 14 | 63 | 64 | 65 | 66 | 67 | 68 | 69 | 70 | 71 | FALLING | 3 |
| 7 | 99 | 100 | 101 | 102 | 103 | 104 | 105 | 106 | 107 | RISING | 4 |
| 15 | 135 | 136 | 137 | 138 | 139 | 140 | 141 | 142 | 143 | FALLING | 4 |
| (1) The mapping
is not sequential. First bit of write_strobe corresponds to the first 9 wdata
bits. The second bit does not correspond to the next 9 wdata bits. | |
Table 5-7. Write Data to Write Strobe Mapping (x9)| WSTRB_MAPPING_INDEX | WDATA INDEX | RISING/FALLING | CLOCK CYCLE |
|---|
| 0 | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | RISING | 1 |
| 1 | 36 | 37 | 38 | 39 | 40 | 41 | 42 | 43 | 44 | FALLING | 2 |
| 2 | 9 | 10 | 11 | 12 | 13 | 14 | 15 | 16 | 17 | RISING | 3 |
| 3 | 45 | 46 | 47 | 48 | 49 | 50 | 51 | 52 | 53 | FALLING | 4 |
| 4 | 18 | 19 | 20 | 21 | 22 | 23 | 24 | 25 | 26 | RISING | 1 |
| 5 | 54 | 55 | 56 | 57 | 58 | 59 | 60 | 61 | 62 | FALLING | 2 |
| 6 | 27 | 28 | 29 | 30 | 31 | 32 | 33 | 34 | 35 | RISING | 3 |
| 7 | 63 | 64 | 65 | 66 | 67 | 68 | 69 | 70 | 71 | FALLING | 4 |