-Wl,-llibrary
Search the library named library when linking.
It makes a difference where in the command you write this option. The linker searches and processes libraries and object files in the specified order. Thus, foo.o -lz bar.o searches library z after file foo.o but before bar.o.
The linker searches a standard list of directories for the library, which is a file named liblibrary.a. The linker then uses this file as if it had been specified precisely by name.
-Wl, Ldir
Add directory dir to the list of directories to be searched for -l.