The Tools Info window shows information about connected tools. At the moment, only the Xplained Pro series is supported.
When a tool is connected, the window will open. It has a short description of the tool, an image of the tool, a section of links to the user guide, relevant data sheets on the internet, etc.
There is also a table with technical details about the tool, such as firmware version, serial number, etc.