This section will introduce the debugging capabilities of Microchip Studio, both as video
(linked below) and hands-on document. The main topics are; breakpoints, basic code
stepping using the Breakpoint and Callstack-Windows and adjusting project compiler
optimization settings.
Getting Started Topics
Video: Microchip Studio Debugging-1
The same code as the one created in section Editor: Writing and Re-Factoring Code (Visual Assist) is used.
Todo: Place a
breakpoint and inspect a list of all breakpoints in the project.
- 1.Set a breakpoint on the line getting the
switch state, as indicated in Figure 1.
Figure 1. Placing a
Breakpoint
Info: A breakpoint can be placed at a
line of code by:
- Clicking the gray bar on the
left edge of the editor window
- In the top menu bar, go to
Debug → Toggle Breakpoint
- By pressing F9 on the
keyboard
- 2.Launch a debug session . The
breakpoint will be hit when clicking the switch (SW0) on the Xplained Pro kit.
Observe that execution halts when hitting the breakpoint, and the execution arrow
indicates that the line of code will execute where the breakpoint is placed. See
Figure 2.
Figure 2. Execution Halting when a
Breakpoint is Hit
Tip: If a
breakpoint is hit in a file that is not currently open, Microchip Studio will
open the file in a temporary pane. A file containing a hit breakpoint in a debug
session will always be in focus.
- 3.Since most of the logic of the program is
handled only when an ISR is processed, it is now possible to check the logical flow
of the program. If the switch is pressed and then released when the ISR is hit -
what will be the state of the switch that the function returns? The assumption is
that since pressing the switch triggered the interrupt, that switch will be set as
pressed, and the LED will thus be turned ON.
Todo: Find out what state is
returned if the switch is pressed and released when hitting the ISR. Is our
assumption correct that since pressing the switch triggered the interrupt,
it will be set as pressed, and the LED will turn ON?
Use the
Step Into Function Call
first.
Use the
Step Out of Function Call
to move
to the following line after returning from the function to enter the SW_get_state( )
function. Pressing
Step Over
from
the breakpoint would land us at this same point directly. Note that we could step
further into the
LED_set_state(SW_state) function to determine if the LED is
turned ON or not. However, we could hover the mouse pointer over the
SW_state
variable to see that it is 0, i.e., the LED will turn OFF. Verify this by stepping
further.
Figure 4. Checking Value of
SW_state Using Mouse Hover
Info: The switch
state is recorded when calling the
SW_get_state( ) function, although the
breakpoint is triggered by the falling edge when pressing the switch. Verify that
SW_state will read 1 when pressing the switch when stepping over
this
line.
- 1.A window or view to keep track of the
breakpoints in a program is needed. The Quick Launch bar performs a search of the
Microchip Studio user interface menus, which is demonstrated below by comparing
Figure 5 and Figure 6. Note that each of the hits in the
Quick Launch bar is from 'break' related entries in the Debug menu.
Figure 5. 'Break' Search in the
Quick Launch Bar
Figure 6. 'Break' Hits in Debug
Menu
Open the Breakpoints window by clicking on the top result (Debug →
Windows → Breakpoints). The Breakpoints window lists all the breakpoints
in the project, along with the current hit count, as depicted in Figure 7.
Tip: Temporarily disable a breakpoint by unchecking the checkbox next to a
breakpoint in the list.
Tip: The Disassembly view can be
conveniently displayed alongside the source code, as demonstrated in
Figure 8.
Figure 7. Breakpoints
Window
Figure 8. Disassembly
View
ToDo: Examine the
Call Stack and the effect on it when optimizations are disabled.
- 1.Following from the previous section, set a
breakpoint on the LED_on() function. Then trigger the
breakpoint so that it is hit.
- 2.Open the Call Stack window by typing 'Call'
in the Quick Launch bar, selecting Debug → Windows → Call Stack, as
shown in Figure 9.
Note: A debug session needs to
be active to open this window.
Figure 9. Open the Call
Stack Window
- 3.Expect the Call Stack showing
LED_set_state() as the caller of
LED_on(), as this is how the code is written.
However, in the Call Stack window, _vector_4 is listed as the caller
(see Figure 10) because of compiler
optimization.
Figure 10. Call Stack with
Optimization
Info: The call order is
different because of the compiler optimization. This code is relatively
simple to follow, and it is possible to understand what is going on even
though the compiler was optimized and made subtle changes to what is
expected. In a more complex project, it can sometimes be helpful to
disable the compiler optimization to track down a bug.
Note: To see why the Call Stack
shows that it comes from
_vector_4 initially, click on
PORTB_PORT_vect and look in the context field for the
definition, as shown in
Figure 11.
Figure 11. __vector_4 Is
the PORTB ISR Vector
- 4.Stop debugging by clicking
the Stop Debugging button or pressing Shift + F5.
- 5.Open the project settings by going to
Project → <project_name> properties or pressing Alt
+ F7. Go to the Toolchain tab on the left menu, as in Figure 12.
- 6.Under AVR/GNU C Compiler →
Optimization, set the Optimization Level to None (-O0)
using the drop-down menu.
Figure 12. Disabling Compiler
Optimizations
Warning: Disabling compiler optimization will result in increased memory
consumption and can cause changes in execution timing, which can be
important to consider when debugging time is a critical code.
- 7.Launch a new debug session
and break code execution inside LED_on().
- 8.Observe the Call Stack. It should now adhere
to how the code is written and list LED_set_state() as
the caller of LED_on(), as shown in Figure 13.
Figure 13. Call Stack Without
Optimization
Tip: Microchip Studio will try to
link the compiled code to the source code as best as possible, but the compiler
optimization can make this challenging. Disabling compiler optimization can help
if breakpoints seem to be ignored during debugging or if the execution flow is
hard to follow during code stepping.
Result: The call stack has now been examined both with and without optimization
enabled.
Code Used for Debugging 1
#include <avr/io.h>
#include <stdbool.h>
#include <avr/interrupt.h>
void LED_on();
void LED_off();
bool SW_get_state();
void LED_set_state(bool SW_state);
int main(void)
{
PORTB.DIRSET = PIN4_bm;
PORTB.OUTSET = PIN4_bm;
PORTB.PIN5CTRL |= PORT_PULLUPEN_bm | PORT_ISC_BOTHEDGES_gc;
sei();
while (1)
{
}
}
#pragma region LED_functions
void LED_on()
{
PORTB.OUTCLR = PIN4_bm;
}
void LED_off()
{
PORTB.OUTSET = PIN4_bm;
}
void LED_set_state(bool SW_state)
{
if (SW_state)
{
LED_on();
}
else
{
LED_off();
}
}
#pragma endregion LED_functions
bool SW_get_state()
{
return !(PORTB.IN & PIN5_bm);
}
ISR(PORTB_PORT_vect)
{
uint8_t intflags = PORTB.INTFLAGS;
PORTB.INTFLAGS = intflags;
bool SW_state = SW_get_state();
LED_set_state(SW_state);
}