Use the
Attach to Target option in the
Debug menu or the attach
icon in the debug
toolbar to attach a target causing Microchip Studio to launch a debug session on the
selected target without uploading a new application or causing a reset. Once the debug
session is established, the core of the target halts, and the current execution position of
the target is mapped to the code in the project, meaning that the state of the target is
kept and is possible to inspect with standard debugging techniques. The program halts in
the current position. Complete run control and symbolic debugging should be available after
a successful attach.
Notes:
- The code in the project, mapped to
the content of the running target, can't verify the correctness of this mapping.
This means that if the project contains code not on the target, then the state and
run control might not reflect the truth, as variables and functions might have
different code locations on the target than in the project.
- The ability to activate a debug
session without resetting a target is architecture-dependent. Not all
architectures support this feature.
Attention: Physically connecting
a debug probe to a target might cause the target to reset, as most debug probes need an
electrical connection to the reset line of the device. Take ordinary electrical
precautions to avoid this.