You can also specify the working directory for the tool or command. For example, if the tool reads file system data from the current directory, the tool requires that certain program components are present in the current directory at start-up.