The Watch window and QuickWatch dialog box are places where you can enter variable names and expressions that you want to watch during a debugging session.
The QuickWatch dialog box enables you to examine a single variable or expression at a time. It helps take a quick look at one value or a larger data structure. The Watch window can store several variables and expressions that you want to view for the debugging session. Microchip Studio has multiple Watch windows, which are numbered Watch1 through Watch4.
A variable name is the simplest expression to enter. If you are debugging native code, you can use register names as well as variable names. The debugger can accept much more complex expressions than that, however. For example, you could enter the following expression to find the average value of three variables:
(var1 + var2 + var3) / 3
The debugger accepts the most valid language expressions in a Watch window. For more information, see Expression Formatting.
If you are programming in native code, you may sometimes need to qualify the context of a variable name or an expression containing a variable name. The context means the function, source file, and module where a variable is located. If you have to do this, you can use the context operator syntax.
Expressions that Affect the State of Your Program
Evaluating some expressions can change the value of a variable or otherwise affect the state of your program. For example, evaluating the following expression changes the value of var1
:
var1 = var2
Expressions that change data are said to have side effects. If you enter an expression that has a side effect into the Watch window, the side effect will occur every time the expression is evaluated by the Watch window. This can produce unexpected results if you are unaware that the expression has side effects. An expression known to have side effects is evaluated only one time when you first enter it. Subsequent evaluations are disabled. You can manually override this behavior by clicking an update icon that appears next to the value.
Unexpected side effects are frequently the result of function evaluation. For example, you could enter the following function call into the Watch window:
PrintFunc1(var1) Func1(var1)
If you call a function from the Watch window or QuickWatch, the function you are calling might change data, creating a side effect. One way to avoid any unexpected side effects from function evaluation is to turn OFF automatic function evaluation in the Options dialog box, disabling automatic evaluation of newer language features, such as properties. However, it is safer.
The Microchip Studio debugger automatically expands common data types to show their most principle elements. You can also add expansions for custom data types.
To Evaluate an Expression in the Watch Window
—or—
Drag a variable to a row in the Watch window.
To Evaluate an Expression in QuickWatch
To Reevaluate a Previous Expression in QuickWatch