Right click on Project or Libraries Node in the project to invoke the 'Add Library' Wizard.
Select Toolchain Libraries Tab; here, you will see the available toolchain libraries for the currently selected toolchain for the project.
Select the libraries which you like to add.
Click OK.
You will also be able to see the new library added in the Toolchain Linker Settings.