Tip:
Ensure you have library projects in the current solution.
Steps to add libraries to an application project:
- 1.Right click on the project, or
‘Libraries’ node in the project, to invoke the 'Add Library' wizard.
- 2.Select the ‘Project Libraries’
tab; all the library projects in the current solution will be listed here.
- 3.Select the library project which
you would like to add.
- 4.Click OK to complete.
Figure 1. Add Library Context
Menu
Figure 2. Add Project Library
Figure 3. View of a Project After Adding
Libraries
Also, see that the library was added as project dependency from Project →
Build Dependencies → Project
Dependencies.
Figure 4. View of Project Dependencies View
After Adding Project Libraries