In the Breakpoints window toolbar, click the Export all breakpoints matching
the current search criteria icon.
- 1.The Save
As dialog box appears.
- 2.In the Save
As dialog box, type a name in the File name
box.
- 3.This is the name of the
XML file that will contain the exported breakpoints. Note the folder path shown at the
top of the dialog box. To save the XML file to a different location, change the folder
path shown in that box or click Browse Folders to browse for a
new location.
- 4.Click
Save.