- 1.Right click on the project, or
‘Libraries’ node in the project, to invoke the 'Add Library' wizard.
- 2.Select the ‘Toolchain Libraries’
tab.
- 3.The list of available toolchain
libraries will be listed here.
- 4.Select the libraries which you
would like to add.
- 5.Click OK to complete.
Figure 1. Add Library Context
Menu
Figure 2. Add Library Dialog
Figure 3. View of a Solution With XC8
Project After Adding Libraries
You can also see the new library added in the Toolchain Linker Settings from the
Project → Properties →
Toolchain tab.
Figure 4. View of Linker Option After
Adding Libraries