AVR® Communication Timeout
Shows the timeout delay used for communication with the back-end. If the watchdog detects that timeout is exceeded,
the back-end is restarted. 20000 ms by default.
AVR® Debugger Path
Shows the AVR Debugger path.
AVR® Debugger Port
Indicates the Windows Comm API Port number used by the AVR debugger. 0 by default.
RPC Transaction Times
Filename to put statistic logging in. This is log data from the communication with the back-end. Empty means no logging. Note that the file must be written to a directory where the user has write permission. E.g., C:/tmp/transactionlog.csv.
User Tool Polling
Use internal port polling method for hardware tool discovery instead of relying on Windows Comm Framework. Must restart Microchip Studio if activated. It may slow down your PC considerably, so use it only if you have errors related to Windows Comm Framework. Disabled by default.