By default, there is no keyboard shortcut to this function. If frequently used,
you might want to add one. To add one, click the
Tools →
Options menu button and go to
Environment
→
Keyboard. Start typing
startwithouttdebugging in the
Show commands containing the input field, and select
Debug.StartWithoutDebugging in the list. Then select the
Press shortcut
keys input field, and press the desired key combination. You can, for example, press
Ctrl+F5. Note that this shortcut is already assigned to the
BreakAll
command. If you choose to override it, press the
Assign button to
assign the new keyboard shortcut. Or, you can select an unused key combination.
Figure 1. Add Keyboard Shortcut