Components are versioned when added to the project. To change the version used, use
this dialog.
There are two options when choosing the component version:
Use a specific version
| Lock the project to a specific version of the component.
|
Use the latest version
| Choose the most recent version of the available component.
|
Figure 1. Change Version
Components are part of the device packs in Microchip Studio. Manage these device packs
using the Device Pack Manager.