This dialog box allows you to specify the formatting settings for the XML Editor. You can access the Options dialog box from the Tools menu.
Attributes
Preserve manual attribute formatting Attributes are not reformatted, which is the default.
Align Attributes Each On Their Own Line
Aligns the second and subsequent attributes vertically to match the indentation of the first attribute. The following XML text is an example of how the attributes are aligned.
<item id = "123-A" name = "hammer" price = "9.95"> </item>
Auto Reformat
On Paste From the Clipboard
Reformats XML text pasted from the Clipboard.
On Completion of End Tag
Reformats the element when the end tag is completed.
Mixed Content
Preserve Mixed Content by Default
Determines whether the editor reformats mixed content. By default, the editor attempts to reformat mixed content, except when the content is found in an xml:space="preserve"
scope.
If an element contains a mix of text and markup, the contents are considered to be mixed content. The following is an example of an element with mixed content.
<dir>c:\data\AlphaProject\ <file readOnly="false">test1.txt</file> <file readOnly="false">test2.txt</file> </dir>