Pressing the Delete Flavor button
deletes the Flavor configuration.
Note: The Native
flavor will be set as default when deleting the customized default flavor. Also, the
projects configured with the deleted flavor will be changed to the default flavor of the
respective toolchain type when opening the project the next time.