-Wl,option
Pass
option
as an option to the linker. If the
option
contains commas, it splits into multiple options at
the commas. You can use this syntax to pass an argument to the option. For
example, `-Wl,-Map,output.map' passes `-Map output.map' to the linker.
-Wl, -nostartfiles
Do not use
the standard system startup files when linking. The standard system libraries
are normally used unless using -nostdlib
or
-nodefaultlibs
.
-Wl,-nodefault
Do not use the
standard system libraries when linking. Onlythe specified libraries will be
passed to the linker. Options specifying linkage of the system libraries, such
as -static-libgcc
or -shared-libgcc
, will be
ignored. The standard start-up files are normally used, unless using
-nostartfiles
. The compiler may generate calls to
memcmp
, memset
, memcpy
,
and memmove
. Entries in libc can solve these entries. These
entry points should be supplied through some other mechanism when this option is
specified.
-Wl,-nostdlib
Do not use the standard system start-up files or libraries when linking.
One of the
standard libraries bypassed by -nostdlib
and
-nodefaultlibs
is libgcc.a
, a library of
internal subroutines that GCC uses to overcome shortcomings of particular
machines or special needs for some languages. In most cases, you need libgcc.a
even when avoiding other standard libraries. In other words, when you specify
-nostdlib
or -nodefaultlibs
, you should
usually specify -lgcc as well, which ensures that you have no unresolved
references to internal GCC library subroutines.
-Wl,-s
Remove all symbol table and relocation information from the executable.
-Wl,-static
On systems that support dynamic linking, this prevents linking with the shared libraries. On other systems, this option has no effect.