To Access the Code Snippets Manager
On the Tools menu, click Code Snippets Manager.
To Add a Directory To the Code Snippet Manager
- 1.In the Language: Drop-down list, select the
language you want to add a directory to.
- 2.Click Add. This opens the Code Snippets Directory window.
- 3.Select the directory you want to add to the Code
Snippets Manager and click OK. The directory will now be used to search for
available code snippets.
To Remove a Directory From the Code Snippet Manager
- 1.Select the directory that you want to remove.
- 2.Click Remove.
To Import a Code Snippet Into the Code Snippet Manager
- 1.In the Language: drop-down list, select the
language you want to add the code snippet to.
- 2.Select the existing folder you want to place the
imported code snippet into.
- 3.Click Import. This opens the Code Snippets Directory window.
- 4.Select the code snippet file you want to add to
the Code Snippets Manager and click OK. The code snippet is now available for
insertion into the code editor.