Sets the default path of Microchip Studio project folders and determines the default behavior of the Output window, Task List, and Solution Explorer as projects are developed and built. To access this dialog box, on the Tools menu, click Options, expand Projects and Solutions, and click General.
Projects Location
Sets the default location where new projects and solution folders and directories are created. Several dialog boxes also use the location given in this option for folder starting points. For example, the Open Project dialog box uses this location for the My Projects shortcut.
User Project Templates Location
Sets the default location used by the New Project dialog box to create the list of My Templates.
User Item Templates Location
Sets the default location used by the Add New Item dialog box to create the list of My Templates.
Always Show Error List if Build Finishes with Errors
Opens the Error List window on build completion only if a project failed to build. Errors that occur during the build process are displayed. When this option is cleared, the errors still occur, but the window does not open when the build is complete. This option is enabled by default.
Track Active Item in Solution Explorer
When selected, Solution Explorer automatically opens, and the active item is selected. The chosen item changes as you work with different files in a project or solution or different components in a designer. When this option is cleared, the selection in Solution Explorer does not change automatically. This option is enabled by default.
Show Advanced Build Configurations
When selected, the build configuration options appear on the Project Property Pages dialog box and the Solution Property Pages dialog box. When cleared, the build configuration options do not appear on the Project Property Pages dialog box and the Solution Property Pages dialog box for projects that contain one configuration or the two configurations debug and release. The build configuration options are shown if a project has a user-defined configuration.
When deselected, the commands on the Build menu, such as Build Solution, Rebuild Solution, and Clean Solution, are performed on the Release configuration. The commands on the Debug menu, such as Start Debugging and Start Without Debugging, are done on the Debug configuration.
Always Show Solution
When selected, the solution and all commands that act on solutions are always shown in the IDE. When cleared, all projects are created as standalone projects, and you do not see the solution in Solution Explorer or commands that act on solutions in the IDE if the solution contains only one project.
Save New Projects When Created
When selected, you can specify a location for your project in the New Project dialog box. When cleared, all new projects are created as temporary projects. When working with temporary projects, you can create and experiment with a project without specifying a disk location.
Warn User When the Project Location is Not Trusted
If you attempt to create a new project or open an existing project in a not fully trusted location (for example, on a UNC path or an HTTP path), a message displays. Use this option to specify whether the message is displayed when you try creating or opening a project in a not fully trusted location.
Show Output Window When Build Starts
Automatically displays the Output Window in the IDE when the solution builds.
Prompt for Symbolic Renaming When Renaming Files
When selected, a message box displays asking whether or not Microchip Studio should also rename all references in the project to the code element.