Microchip Studio for AVR® and SAM Devices 7.0.2594
- Support for MPLAB® PICkit™ 4 with a firmware
update
- Updated debugger firmware for device support
with Atmel-ICE, JTAGICE3, and Power Debugger
- Support for project import of MPLAB® Code
Configurator generated projects
- Advanced Software Framework 3.52.0,
including previous version back to 3.44.1
Microchip Studio for AVR® and SAM Devices 7.0.2542
- Renaming of Atmel Studio to Microchip Studio for AVR and SAM Devices
- Microchip Studio installer bundles with the AVR GCC Toolchain, Arm GCC
Toolchain, and the MPLAB® XC8 Compiler with AVR devices support. To unlock
all optimization options of the MPLAB XC8 Compiler, try or get a PRO
license.
- Default optimization for debug configuration is -Og, previous it was
-O1
- Improved scrolling performance on large projects/files
- AVR Macro assembler version 2.2.8
- Advanced Software Framework 3.49.1, including previous version back to
3.42
- Updated kit recognition
Atmel Studio 7.0.2397
- Updated nEDGB firmware (v1.14.464) fixing a connection issue
Atmel Studio 7.0.2389
Atmel Studio 7.0.2389 contains:
- Advanced Software Framework 3.47.0
- AVR 8-bit GCC Toolchain 3.6.2
- Arm GCC Toolchain 6.3.1 with Upstream
Versions: GCC (Arm/embedded-6-branch revision 249437), GNU Arm Embedded
Toolchain: 6-2017-q2-update
- Inclusion of the Most Recent Device Family
Packs Included in Installer as of Sept. 2019. Use the Device Pack Manager to
Check for Updates to get the Newest Device Support or Download an Older
Device Family Pack for Legacy Support.
- Contains Fixes for the Following Issues:
- AVRSV-8221: Issue
with SRAM access seen for ATtiny817 with EDBG
- AVRSV-8212: Reading
Target voltage for SAMD21 fails
- AVRSV-8187: Support
for CMSIS 5.4.0 schema in atpackmanager
- AVRSV-8170: SAM D51, E5x - ELF parsing
incorrect with ECC in Flash
- AVRSV-8105: Erase
User page before programming fails for SAME54
- AVRSV-8073: SAM E54
User Page read/write using atprogram
- AVRSV-8130: Studio picks up old
JLinkArm.dll instead of the installed one
- AVRSV-8166: tinyAVR®-2 devices are not compiling due to incorrect memory
definition in a linker script
- AVRSV-8176: EEPROM
and User Signature erase broken on UPDI
- AVRSV-8158: Unable to
build ASM-projects for AVR64DA128 in Studio
- AVRSV-8123: Reading
voltage doesn't work when device ID does not match
- AVRSV-8152: Update
lib-elf-dwarf build job from stash to bitbucket
- AVRSV-8132: ChipErase issue with
J-Link
- AVRSV-8131:
SAMD21J17D is unable to Program or Debug with Atmel-ICE
- AVRSV-8171: SAM L11
BOOTOPT programming issue
- AVRSV-8159: Not able
to program BOCOR on SAML11 from within an ELF file
- AVRSV-8149: Breakpoints support for
TrustZone SG assembly instruction
- AVRSV-8182: Issue
with Secure Boot support for SAM L11
Atmel Studio 7.0.1931
Atmel Studio 7.0.1931 contains:
- Advanced Software Framework
3.40.0
- New Microchip Gallery
extension
- Atmel START Extension
Provides Improved Feedback on Required Device Pack Dependencies
- Support for Arm®
Cortex®-M23 Architecture with TrustZone
- Support for Kits with the New
nEDBG Debugger Platform
- Support for Devices:
- ATSAMHA1E[14|15|16]AB
- ATSAML10[D|E][14|15|16]A
- ATSAML11[D|E][14|15|16]A
- ATtiny202, ATtiny204,
ATtiny402, ATtiny404, ATtiny406, ATtiny804, ATtiny806, ATtiny807,
ATtiny1604, ATtiny1606, ATtiny1607
- AVR 8-bit GCC Toolchain 3.6.1
- Arm GCC Toolchain 6.3.1 with Upstream
Versions: GCC (Arm/embedded-6-branch revision 249437), GNU Arm Embedded
Toolchain: 6-2017-q2-update
- Atmel Studio 7.0.1931
Contains Fixes for the Following Issues that were Present in 7.0.1645:
- AVRSV-8001: Tool
firmware upgrade instability.
- AVRSV-8063: ELF production file
programming did not support fuses for the ATtiny817 family.
- AVRSV-8075: Launch of
debugging with ATSAM4L unstable in some cases.
- AVRSV-7895: Solution with links between
projects compiles the wrong file.
- AVRSV-7745: Linked files in a subfolder
cause build failure.
- AVRSV-7939: Function
breakpoint fails for AVR devices.
- AVRSV-8005: Writing fuses and memory
sometimes fails cases on M0+ devices.
Atmel Studio 7.0.1645
Atmel Studio 7.0.1645 contains:
- Advanced Software Framework
3.35.1.898
- Support for Devices:
- ATmega4808,
ATmega4809
- ATtiny1614,
ATtiny3214, ATtiny3216, ATtiny3217
- ATSAMC[20|21][J|N][15|17|18]A
- ATSAMD20[E|G|J][14|15|16]B
- ATSAMD51[G|J|N|P][18|19|20]A
- ATSAME[51|53|54][J|N][18|19|20]
- ATSAME70[N|Q][19|20|21]B
- ATSAMS70[J|N|Q][19|20|21]B
- AVR 8-bit GCC Toolchain
3.6.1
- Arm GCC Toolchain 6.3.1 with Upstream
Versions: GCC (Arm/embedded-6-branch revision 249437), GNU Arm Embedded
Toolchain: 6-2017-q2-update
- Atmel Studio 7.0.1645
Contains Fixes for the Following Issues that were Present in 7.0.1417:
- AVRSV-7798: ATtiny817 fuse programming
from the ELF issue fixed.
- AVRSV-7742: Compiling an imported Arduino
sketch for Arduino zero shows an error.
- AVRSV-7903: Studio automatically sets
GPNVM bits [7:8], thereby enabling TCM.
- AVRSV-7892: Writing SAML22 RWW Flash
fails.
- AVRSV-7889: Skewed
debug info for AVR 8-bit in AS 7.0.1417.
- AVRSV-7883: Incorrect warning message for
KB2978092 during the installation of AS 7.0.1417.
- AVRSV-7106: Hex
parser fails on UNIX® line
endings.
- AVRSV-4914: Add
support for new avr-gcc __int24 and __uint24 types.
- AVRSV-7877: Devices
with external SRAM fails to calculate available SRAM.
- AVRSV-7845: Crash in
_ReallyTerminateAfterLaunchFinished.
- AVRSV-7834: Pack
manager fails to download CMSIS DFPs.
- AVRSV-7876: Add checksum fields to the
http header for KitsDatabase.xml.
- AVRSV-7854: NaN
values not handled by atprogram.
- AVRSV-7911: Problems
reading device ID on ATmega4809.
- AVRSV-7202: Arduino Library Grouping can
have a better representation.
- AVRSV-7927: Security Bit Window in Device
Programming may not always be available depending on the MCUs.
- AVRSV-7973: Chip
erase outside prog session fails on SAM4L.
- AVRSV-7961: FUSE
configuration warning for BOD( BODCFG.LVL) is incorrect in Atmel
Studio.
Note: QTouch® Composer extension must be updated to version
5.9.122 or later to work with Atmel Studio 7.0.1645.
Atmel Studio 7.0.1417
Atmel Studio 7.0.1417 contains a fix for the following issue that was present in
7.0.1416:
- AVRSV-7827: New WinUSB driver fails to
install on 32-bit Windows®
Atmel Studio 7.0.1416
The following changes are done in Atmel Studio 7.0.1416:
- Changed Driver to WinUSB for
AVR Dragon, AVRISP mkII, JTAGICE mkII, JTAGICE3, AVR ONE!, STK600, and
QT600
- Installer Improvements
- Improved Support for
Installing Older Device Family Packs
- AVR 8-bit GCC Toolchain 3.6.0
with Upstream Versions:
- GCC 5.4.0
- Binutils
2.26.20160125
- avr-libc 2.0.0
- gdb 7.8
- Arm GCC Toolchain 6.2.1 with Upstream
Versions:
- GCC (Arm/embedded-6-branch revision
243739), GNU Arm Embedded Toolchain: 6-2016-q4-major
- Binutils 2.27
- gdb 7.12
- Advanced Software Framework
3.34.1
Atmel Studio 7.0.1416 contains a fix for the following issues that were present in
7.0.1188:
- AVRSV-7492: Illegal PC value
after a few resume-suspend cycles on SAMD10.
- AVRSV-7486: Debugging may fail in Cortex®-M0+ SAM devices at a high clock.
- AVRSV-7693: Go to source from
Watch window crashes studio.
- AVRSV-7741: Writing Flash or EEPROM with a
size of 0x100 or 0x1000 fails on ISP/SPI programming.
Atmel Studio 7.0.1188
The following changes are done in Atmel Studio 7.0.1188:
- Added Support for New AVR8X
Architecture
- Installer Improvements
- Improved Arduino Import
- Change How Fuses are listed in the
Programming Dialog
- AVR 8-bit GCC Toolchain 3.5.4 with Upstream
Versions:
- GCC 4.9.2
- Binutils 2.26
- avr-libc 2.0.0
- gdb 7.8
Atmel Studio 7.0.1188 Contains a Fix for the Following Issues that were Present in
7.0.1006:
- AVRSV-7149: When writing
EEPROM, bytes that are 0xFF are wrongly skipped.
- AVRSV-7393: Atmel Studio
backend crashes when debugging a COFF object file.
- AVRSV-7564: Atmel Studio
installation is hanging.
- AVRSV-7580: Atmel Studio not
handling DCACHE properly on SAM Cortex®-M7
devices.
- AVRSV-7582: Remove white spaces while saving
the file does not show the anticipated effect.
- AVRSV-7594: Atmel Studio
crashes in some cases when you stop debugging.
- AVRSV-7602: Cannot find
bounds of the current function.
- AVRSV-7607: Invalid MTB
buffer start address for SAML2x and SAMC2x devices.
Atmel Studio 7.0.1006
The following changes are done in Atmel Studio 7.0.1006:
- New Atmel START Extension That Allows the
User to Create and Configure Atmel START Projects within Atmel Studio
- Ability to Load Multiple Modules in a Debug
Session (experimental)
- AVR 8-bit GCC Toolchain 3.5.3 with Upstream
Versions:
- GCC 4.9.2
- Binutils 2.26
- avr-libc 2.0.0
- gdb 7.8
- Arm GCC Toolchain 5.3.1 with Upstream
Versions:
- GCC (Arm/embedded-5-branch revision
234589)
- Binutils 2.26
- gdb 7.10
Atmel Studio 7.0.1006 Contains a Fix for the Following Issues that were Present in
7.0.943:
- AVRSV-6878: Atmel Studio
write the write-once wdt registers on some SAM devices.
- AVRSV-7470: SAM Cortex®-M7 devices fail to launch occasionally.
- AVRSV-7471: Devices with external and
internal RAM list all the available RAM.
- AVRSV-7473: Atmel Studio
hangs during start-up.
- AVRSV-7474: Kits connected to
Atmel Studio are not getting enumerated in the QTouch Start Page.
- AVRSV-7477: Show all files that do not work
from solution explorer.
- AVRSV-7482: Exception when
adding a breakpoint on SAM4L.
- AVRSV-7486: Debugging may
fail in Cortex®-M0+ SAM devices at high
clock speeds.
Atmel Studio 7.0.943
Atmel Studio 7.0.943 contains a fix for the following issue:
- AVRSV-7459: Projects containing files with
uppercase filenames can fail to build. Saving files with uppercase filenames
convert filenames to lower case.
Atmel Studio 7.0.934
The following changes are done in Atmel Studio 7.0.934:
- AVR 8-bit GCC Toolchain 3.5.2 with Upstream
Versions:
- GCC 4.9.2
- Binutils 2.26
- avr-libc 2.0.0
- gdb 7.8
- AVR 32-bit GCC Toolchain 3.4.3 with Upstream
Versions:
- GCC 4.4.7
- Binutils 2.23.1
- Newlib 1.16.0
- Arm GCC Toolchain 4.9.3 with Upstream
Versions:
- GCC (Arm/embedded-4_9-branch revision
224288)
- Binutils 2.24
- gdb
7.8.0.20150304-cvs
Atmel Studio 7.0.934 resolves the following issues present in Atmel
Studio 7.0.790:
- AVRSV-7376: Atmel-ICE slow
programming.
- AVRSV-7379: Unhandled
exception when writing fuses or lock bits when Auto Read is turned off.
- AVRSV-7396: Some machines show an error
regarding 'Exception in MemoryPressureReliever'.
- AVRSV-7400: When in Standard mode,
Disable debugWIRE and Close are not visible in
the Debug menu.
- AVRSV-7408: When using Atmel
Studio in Standard mode, the Set Startup Project menu
is missing.
Atmel Studio 7.0.790
The following features are added in Atmel Studio 7.0.790:
- Support for Mass Storage Mode in Embedded
Debugger (EDBG), Enabling Drag and Drop Programming
- Introduction of User Interface Profiles. The
User can Choose an Interface Where Some Toolbar Buttons and Menu Items are
Removed.
- Support for Importing Libraries to
Previously Imported Sketches. Added support for Arduino Zero and Zero
Pro.
- Parallel Build Turned on by Default
Atmel Studio 7.0.790 resolves the following issues present in Atmel
Studio 7.0.634:
- AVRSV-7084: Persist user
settings during the upgrade.
- AVRSV-7014: Some ATmega and
ATtiny devices failed to start debugging with the Simulator.
- AVRSV-7230: 'Show all files' in Solution
Explorer is not consistent.
- AVRSV-7062: Firmware upgrade
of Xplained Mini kits not detected.
- AVRSV-7164: Reading Flash to .bin file
created incorrect .bin file.
- AVRSV-7106: Hex files with
UNIX or mixed file endings fail to load.
- AVRSV-7126: Data breakpoints for Arm may not
be limited to RAM.
Atmel Studio 7.0.634
This release adds device support for the SAM B11 device family.
Atmel Studio 7.0.634 resolves the following issues present in Atmel Studio
7.0.594:
- AVRSV-6873: Jungo Driver
issue with Windows 10.
- AVRSV-6676: Launching debugging fails due to
an issue with the Intel graphics driver.
Atmel Studio 7.0.594
Atmel Studio 7.0.594 resolves the following issues present in Atmel Studio
7.0.582:
- AVRSV-7008: Opening a 6.2
project in Atmel Studio 7.0.582 persists Debug configuration settings for
all the other configurations.
- AVRSV-6983: Uninstalling
Studio extensions does not work in some cases.
- AVRSV-7018: Project Creation fails with some
culture-specific user names.
- AVRSV-7019: Help Viewer does
not work on 32-bit machines.
- Issues with getting
tools/debuggers recognized or visible see section 2.4 in ‘Atmel Studio
7.0.594-readme.pdf’ for workarounds.
Atmel Studio 7.0.582
- Updated to Visual Studio
Isolated Shell 2015
- Integration with Atmel
START
- This tool will help you select and
configure software components, drivers, middleware, and example
projects to tailor your embedded application in a usable and
optimized manner
- New Device Support System, CMSIS Pack
Compliant
- Data Visualizer, Used for Processing and
Visualizing Data
- Updated Help System, Improved
Context-Sensitive Help
- Advanced Software Framework Version 3.27.3.
ASF is an Extensive Software Library of Software Stacks and Examples.
- A Major Upgrade of the Visual Assist
Extension to Atmel Studio that Assists with Reading, Writing, Re-Factoring,
Navigating Code Fast
- Import Arduino Sketch Projects Into Atmel
Studio
- Support for Flip-Compatible Bootloaders in
atprogram and Programming Dialogue. The Connected Device Appears as a
Tool.
- AVR 8-bit GCC Toolchain 3.5.0 with Upstream
Versions1:
- GCC 4.9.2
- Binutils 2.25
- avr-libc
1.8.0svn
- gdb 7.8
- AVR 32-bit GCC Toolchain 3.4.3 with Upstream
Versions1:
- GCC 4.4.7
- Binutils 2.23.1
- Newlib 1.16.0
- Arm GCC Toolchain 4.9.3 with Upstream
Versions1:
- GCC 4.9 (revision 221220)
- Binutils 2.24
- gdb
7.8.0.20150304-cvs