- 1.Right click on the project, or
‘Libraries’ node in the project, to invoke the 'Add Library' wizard.
- 2.Select the ‘Browse Libraries’
tab.
- 3.Click on the ‘Browse’ button from
the panel to browse and add libraries
- 4.After adding the libraries,
library name, with path, will be listed here
- 5.Click OK to complete.
Figure 1. Add Library Context Menu
Figure 2. Browse Libraries