Getting Started With the QTouch® Composer in Microchip Studio on YouTube.
QTouch Project builder will guide you through all steps from selecting device and touch sensors
to automatically generating a complete touch project.
- 1.Start Microchip Studio.
- 2.Open the File menu. Click on 'New → Project'.
- 3.The 'New Project' dialog is opened. Select 'GCC C
QTouch Executable Project' in the New Project dialog.
Enter the
following details in the 'New Project' dialog and click the OK button:
- Name of the project
- Location of the project and
solution
- Name of the solution
- 4.The 'QTouch Project Builder' wizard is opened, which will guide you through the steps involved in creating a project.