When the application program writes a byte of data to the OCDR
register of
an AVR device while being debugged, the debugger reads this value out and displays it as
IDR events in the output window, as shown in the figure below. The OCDR
register is polled at a given interval, so writing to it at a higher frequency than the one
specified for the debugger will not yield reliable results. The device data sheet will
explain how to check that a given value has been read.
IDR Messagesdrop-down if no IDR events have been sent from the debugger.