This Options page allows you to add, delete, and change the comment tokens that generate Task List reminders. Select Options from the Tools menu, expand the Environment folder, and choose Task List to display these settings.
Confirm Deletion of Tasks
When selected, a message box is displayed whenever a User Task is deleted from the Task List, allowing you to confirm the deletion. This option is selected by default.
Hide Full File Paths
When selected, the File column of the Task List displays only the names of files to be edited, not their full paths.
Tokens
When you insert a comment into your code whose text begins with a token from the Token List, the Task List displays your comment as a new entry whenever the file is opened for editing. You can click this Task List entry to jump directly to the comment line in your code.
Token List
Displays a list of tokens and allows you to add or remove custom tokens. Comment tokens are case-sensitive.
Priority
Sets the priority of tasks that use the selected token. Task comments that begin with this token are automatically assigned the designated priority in the Task List.
Name
Enter the token string, which enables the Add button. On Add, this string is included in the Token List, and comments that begin with this name will be displayed in the Task List.
Add
Enabled when you enter a new Name. Click to add a new token string using the values entered in the Name and Priority fields.
Delete
Click to delete the selected token from the Token List. You cannot delete the default comment token.
Change
Click to change an existing token using the values entered in the Name and Priority fields.