-llibrary
The
-llibrary option scans the library named
library for unresolved symbols when
linking. The linker searches a standard list of
directories for the library with the name
library.a. It makes a difference
where you write this option in the command. The
linker processes libraries and object files in the
order they are specified. Thus, foo.o -lz
bar.o
searches library z after
file foo.o but before bar.o. If
bar.o refers to functions in libz.a,
those functions may not be loaded.
The directories searched include several standard system directories, plus those specified with -L.
Usually, the files found this way are library files (archive files whose members are object files). The linker handles an archive file by scanning through it for members, which define symbols that have been referenced but not defined yet. But if the file found is an ordinary object file, it is linked in the usual fashion. The only difference between using an -l option (e.g., -lmylib) and specifying a filename (e.g., mylib.a) is that the compiler will search for a library specified using -l in several directories as specified by the -L option.
-Ldir
Add a directory to the list of directories to be searched for -L.