The Data Breakpoint window provides the options to set data breakpoints and lists the added data breakpoints. Enable this window by choosing Debug → Windows → Data Breakpoints.
The Data Breakpoints toolbar has the following elements:
The Data Breakpoints window displays several columns related to the breakpoint configuration. Some of the columns are dynamically hidden based on the breakpoints configuration. E.g., if none of the breakpoints have Mask-configured, then Mask-related columns are not displayed.
The Name column has three parts:
Icon | Description |
---|---|
Normal breakpoint. The solid glyph indicates that the breakpoint is enabled. The hollow glyph indicates that it is disabled. |
|
Advanced breakpoint. Active/disabled. The + sign indicates that the breakpoint has a hit count attached to it. |
|
Tracepoint. Active/disabled. Hitting this point performs a specified action but doesn't break the program execution. |
|
Advanced tracepoint. Active/disabled. The + sign indicates that the tracepoint has hit count attached to it. |
|
Breakpoint or tracepoint error. The X indicates that the breakpoint or tracepoint couldn't be set because of an error condition. Check the Message column for more details on the error message. |
|
Breakpoint or tracepoint is set but with a warning. Check the Message column for more details on the warning message. |