12.14 Advertising Timing Parameters
In Auto Operation mode, the advertising timing parameters, along with the power-on standby time and disconnect standby time, define how often and how long the BM70/71 module advertises its presence. For more details on different advertising intervals, refer to the BM70/71 Bluetooth® Low Energy Module User’s Guide (DS50002542).
In Manual Operation mode, the external host MCU uses specific commands to control when and how often the IS187x device advertises its presence. The user can ignore the parameters when Manual Operation mode is active (see the following table). For more details, refer to the BM70/71 Bluetooth® Low Energy Module User’s Guide (DS50002542).
In Auto Operation mode, if programming values are not within the valid ranges, undefined device operation will result (see the following table).
| Parameter | Value | Parameter Description | Length |
|---|---|---|---|
| 0x3D-0x3E | 0xXXXX |
| 2 bytes |
| Parameter | Value | Parameter Description | Length |
|---|---|---|---|
| 0x3F-0x40 | 0xXXXX |
| 2 bytes |
| Parameter | Value | Parameter Description | Length |
|---|---|---|---|
| 0x41 | 0xXX |
Note: This can cause the IS187x device to consume more current.
| 1 byte |
Operational Mode
The IS187x device only uses the advertising timing parameters when working in Auto Operation mode.