12.1 Name Fragment
This is the ASCII string, where the user can program the device to set the name of the device. Use this string during advertising. It must match the value programmed into the advertising data structure configuration parameter. For more details, refer to Advertising Data Structure.
| Parameter | Value | Parameter Description | Length |
|---|---|---|---|
| 0x0006-0x0026 | 0xXX | This is the ASCII string a user can program into the device to set the name of the device. This string is used when the device is advertising. | 32 bytes |
Operational Mode
Use the name fragment configuration parameter in both Manual and Auto Operation mode. In Manual Operation mode, the host MCU can override the programmed value by using the appropriate command from the command set protocol.