12.2 HCI UART Baud Rate
Use the HCI UART baud rate value to set the baud rate of the IS187x device that is used for communication over the HCI UART. After making a change, the new baud rate only takes affect after a device reset.
Use the programmed baud rate in all modes of device operation, such as:
- Direct test
- Firmware programming
- Device configuration
- Run (Auto/Manual Operation) modes
| Parameter | Value | Parameter Description | Length |
|---|---|---|---|
| 0x27 | 0xXX | The following are the possible values:
| 1 byte |
Operational Mode
Use the HCI UART baud rate parameter in both Manual and Auto Operation mode.