12.3 RF Class
The following table provides details about the RF class configuration parameter.
| Parameter | Value | Parameter Description | Length |
|---|---|---|---|
| 0x28 | 0xXX | This is a hex value representing the RF class type to be used by the device. The following are the possible values:
| 1 byte |
Operational Mode
This value does not affect Manual or Auto Operation mode.