12.11 Configure Timeout
The configure timeout parameter represents the period when the external host MCU can send a command set protocol message to the IS187x device. This parameter only works when auto Operation mode is active. For details on why an external host MCU wants to use this option, refer to the BM70/71 Bluetooth® Low Energy Module User’s Guide (DS50002542).
| Parameter | Value | Parameter Description | Length |
|---|---|---|---|
| 0x31 | 0xXX |
| 1 byte |
Operational Mode
The configure timeout parameter is applicable in Auto Operation mode.