9.2.5 IS2062GM-SAC305

The following figure illustrates the package details of the IS2062GM-SAC305.

Figure 9-6. IS2062GM-SAC305 PACKAGE DETAILS
Note: For the most current package drawings, see the Microchip Packaging Specification located at http://www.microchip.com/packaging.