17.4.2.7 Leading-Edge Blanking
The Leading-Edge Blanking (LEB) feature is used to mask transients that could otherwise cause an erroneous Fault condition. Leading-Edge Blanking can be implemented using any of the PCI blocks and basically ‘ignores’ an input signal for a specified time following a PWM edge event.
Both the rising and falling edges of both PWMxH and PWMxL signals can be selected to start the LEB timer. The LEB time duration is set by writing a value to the LEB bits (PGxLEBL[15:3]). More than one edge (PHR, PHF, PLR or PLF; refer to the PGxLEB register) may be used; however, if timing overlaps, the counter will be reset on each valid edge. In most applications, only one edge of the PWM signal needs to be selected to trigger the LEB timer.
The LEB counter is commonly used to avoid a false trip when the PCI logic is used for current limiting. In this scenario, the LEB counter can be triggered on both edges of the PWM signal. The PCI logic is operated in Latched Acceptance mode with the LEB active signal used as a disqualifier to the PCI input signal. Figure 17-31 shows a PWM cycle where a PCI input goes active during the LEB timer. There is no PCI active event or output override until the LEB timer has expired.