2.105.16 SDHCx_ResponseRead Function
C
/* x = SDHC instance number (x is applicable only on devices with more than one instances of SDHC) */ void SDHCx_ResponseRead ( SDHC_READ_RESPONSE_REG respReg, uint32_t* response )
Summary
Reads the specified response into the application response buffer
Description
If the command requires a response, it can be read using this API.
Precondition
A command having a response must have been submitted using the SDHCx_CommandSend() function.
Parameters
| Param | Description |
|---|---|
| respReg | Enumeration identifying the response type to read |
| response | Pointer to the buffer to read the response into |
Returns
None.
Example
uint32_t cmd_response;
SDHC1_ResponseRead(SDHC_READ_RESP_REG_0, &cmd_response);
Remarks
None.