2.105.4 SDHCx_BlockSizeSet Function
C
/* x = SDHC instance number (x is applicable only on devices with more than one instances of SDHC) */ void SDHCx_BlockSizeSet ( uint16_t blockSize )
Summary
Sets the size of the one data block of transfer.
Description
Sets the size of the one data block of transfer.
Precondition
SDHCx_Initialize() must have been called first for the associated instance.
Parameters
| Param | Description |
|---|---|
| blockSize | Size of one block of transfer |
Returns
None.
Example
SDHC1_BlockSizeSet(512);
Remarks
None.