2.105.9 SDHCx_IsCardAttached Function
C
/* x = SDHC instance number (x is applicable only on devices with more than one instances of SDHC) */ bool SDHCx_IsCardAttached ( void )
Summary
Indicates if the card is attached or detached
Description
Indicates if the card is attached or detached
Precondition
SDHCx_Initialize() must have been called first for the associated instance.
Parameters
None.
Returns
true - If the card is inserted.
false - If the card is removed.
Example
if (SDHC1_IsCardAttached() == true)
{
// Card is attached
}
Remarks
None.