2.105.20 SDHCx_DmaSetup Function
C
/* x = SDHC instance number (x is applicable only on devices with more than one instances of SDHC) */ void SDHCx_DmaSetup ( uint8_t* buffer, uint32_t numBytes, SDHC_DATA_TRANSFER_DIR direction )
Summary
Sets up the DMA for data tranfers.
Description
The client of the SDHC PLIB must set up the DMA before initiating a data transfer.
Precondition
SDHCx_Initialize() must have been called first for the associated instance.
Parameters
| Param | Description |
|---|---|
| buffer | Pointer to the read or write buffer (depending on the direction argument) |
| numBytes | Number of bytes to read or write |
| direction | Direction of the data transfer, SDHC_DATA_TRANSFER_DIR_READ or SDHC_DATA_TRANSFER_DIR_WRITE. |
Returns
None.
Example
uint8_t readBuffer[512]; SDHC_DataTransferFlags transferFlags; transferFlags.isDataPresent = true; transferFlags.transferDir = SDHC_DATA_TRANSFER_DIR_READ; transferFlags.transferType = SDHC_DATA_TRANSFER_TYPE_SINGLE; // Set up the DMA to read 512 btyes of data SDHC1_DmaSetup(readBuffer, 512, SDHC_DATA_TRANSFER_DIR_READ); // Send command to read one block of data from SD card starting at block address 100 SDHC1_CommandSend(17, 100, SDHC_CMD_RESP_R1, transferFlags);
Remarks
None.