2.91.10 QEIx_Disable Function
C
/* x refers to the instance number */
inline static void QEIx_Disable(void)
Summary
This inline function disables the QEIx peripheral.
Description
This function disables the instance of the QEI peripheral by clearing the enable bit in the QEIxCON register.
Precondition
QEI peripheral should be initialized and enabled properly.
Parameters
None.
Returns
None.
Example
QEI1_Initialize();
QEI1_Enable();
//Perform QEI1 operations here
QEI1_Disable();
Remarks
Stops the execution of the QEIx peripheral