2.92.9 QMSPIx_DMATransferRead Function
C
// x - Instance of the QMSPI peripheral
uint32_t QMSPIx_DMATransferRead(QMSPI_DESCRIPTOR_XFER_T *qmspiDescXfer, void* pReceiveData, size_t rxSize);
Summary
Reads data from the QMSPI slave device.
Description
This function can be used to read n bytes of data from the specified address of the serial flash device connected as a QMSPI slave.
Precondition
QMSPIx_Initialize must have been called for the associated QMSPI instance.
Parameters
| Param | Description |
|---|---|
| *qmspiDescXfer | Pointer to QMSPI descriptor transfer structure. |
| *pReceiveData | Pointer to receive buffer where the data read from memory will be stored. |
| rxSize | Number of bytes to read. |
Returns
Number of bytes read from memory.
Example
QMSPI_DESCRIPTOR_XFER_T qmspiDescXfer;
memset(&qmspiDescXfer, 0x00, sizeof(QMSPI_DESCRIPTOR_XFER_T));
qmspiDescXfer.address = address;
qmspiDescXfer.qmspi_ifc_mode = QUAD_OUTPUT;
qmspiDescXfer.ldma_enable = true;
qmspiDescXfer.ldma_channel_num = QMSPI_LDMA_CHANNEL_0;
qmspiDescXfer.command = APP_CMD_MEMORY_FAST_READ_QUAD;
qmspiDescXfer.num_of_dummy_byte = 4;
QMSPI0_DMATransferRead(&qmspiDescXfer, pReadBuffer, nBytes);