2.92.8 QMSPIx_DMATransferWrite Function
C
// x - Instance of the QMSPI peripheral
uint32_t QMSPIx_DMATransferWrite(QMSPI_DESCRIPTOR_XFER_T *qmspiDescXfer, void* pTransmitData, size_t txSize);
Summary
Writes data to the QMSPI slave device.
Description
This function can be used to write maximum of one page of data to the specified address of the serial flash device connected as a QMSPI slave. If the number of bytes to be written is greater than the page size then QMSPIx_DMATransferWrite API needs to be called multiple times.
Note: Before sending next write request, QMSPIx_Read() can be called to read the status register of the slave device to check if the previous write operation is completed.
Precondition
QMSPIx_Initialize must have been called for the associated QMSPI instance. Write enable command has to be sent before write memory request.
Parameters
| Param | Description |
|---|---|
| *qmspiDescXfer | Pointer to QMSPI descriptor transfer structure. |
| *pTransmitData | Pointer to transmit buffer holding the data to write into memory. |
| txSize | Number of bytes to write. |
Returns
Number of bytes written in memory.
Example
uint32_t i;
QMSPI_DESCRIPTOR_XFER_T qmspiDescXfer;
APP_WriteEnable();
memset(&qmspiDescXfer, 0x00, sizeof(QMSPI_DESCRIPTOR_XFER_T));
qmspiDescXfer.command = APP_CMD_QUAD_INPUT_PAGE_PROGRAM;
qmspiDescXfer.address = address;
qmspiDescXfer.qmspi_ifc_mode = QUAD_OUTPUT;
qmspiDescXfer.ldma_enable = true;
qmspiDescXfer.ldma_channel_num = QMSPI_LDMA_CHANNEL_0;
for (i = 0; i < APP_PAGE_PROGRAM_SIZE_BYTES; i++)
{
appData.transmitBuffer[i] = pPageData[i];
}
QMSPI0_DMATransferWrite(&qmspiDescXfer, appData.transmitBuffer, APP_PAGE_PROGRAM_SIZE_BYTES);