| 0x00 | The sensor has been disabled and will not perform
measurements |
| 0x01 | The sensor is in an initialized state and has yet to complete
the calibration |
| 0x02 | The sensor is currently being calibrated |
| 0x03 | Touch not detected |
| 0x04 | A confirmation scan is being performed to confirm a
touch |
| 0x85 | No touch is detected |
| 0x86 | A confirmation scan is being performed to confirm a touch
removal |
| 0x07 | Away-from-touch recalibration is being performed for the
sensor |
| 0x08 | The sensor is in a suspended state |
| 0x09 | The calibration process failed for the sensor |
|
Note: Bit 7 is set in each state where the
sensor is “In Detect”.
|