29.6.5 I2C Host Mode Repeated Start Condition Timing
A Repeated Start condition (Figure 29-27) occurs when the RSEN
bit is programmed high and the host state machine is no longer active. When the
RSEN bit is set, the SCL pin is asserted low. When the SCL pin is sampled low, the
Baud Rate Generator is loaded and begins counting. The SDA pin is released
(brought high) for one Baud Rate Generator count (TBRG). When the Baud
Rate Generator times out, if SDA is sampled high, the SCL pin will be deasserted
(brought high). When SCL is sampled high, the Baud Rate Generator is reloaded and
begins counting. SDA and SCL must be sampled high for one TBRG. This
action is then followed by assertion of the SDA pin (SDA = 0
) for one TBRG while SCL is
high. SCL is asserted low. Following this, the RSEN bit will be automatically
cleared and the Baud Rate Generator will not be reloaded, leaving the SDA pin held
low. As soon as a Start condition is detected on the SDA and SCL pins, the S
bit will be set. The SSPxIF bit will not be set until the Baud Rate Generator has
timed out.
- If RSEN is programmed while any other event is in progress, it will not take effect.
- A bus collision during the Repeated Start
condition occurs if:
- SDA is sampled low when SCL goes from low-to-high.
- SCL goes low before SDA is asserted
low. This may indicate that another host is attempting to
transmit a data ‘
1
’.
![](GUID-1D20235B-D45D-4A25-92E6-9039D31F3D6C-low.png)