3.2.25 DIAG_SUPC
The DIAG_SUPC module is designed to verify the correct functionality of the Supply Contrller (SUPC) through a set of C function calls.
The DIAG_SUPC software test API is mapped to the following safety mechanisms:
| Function | Diagnostic Mechanism | Use Case | Elapsed Time (μs)~ |
|---|---|---|---|
| DIAG_SUPC_SFRReset() | SFR_RESET | POST | 20.84 |
| DIAG_SUPC_SFRWriteRead() | SFR_WRITE_READ | POST / OnDemand | 16.62 |
Configuring the Diagnostic
DIAG_SUPC does not require additional configuration.
Run-time Pre-requisites
DIAG_SUPC_SFRRead should be executed before DIAG_SUPC_SFRWriteRead
Using the Diagnostic
#include "definitions.h"
DIAG_TEST_STATUS DIAG_SUPC_SFRPost()
{
DIAG_TEST_STATUS result;
result = DIAG_SUPC_SFRReset(NULL,0,false);
if (result == DIAG_TEST_PASSED)
{
result = DIAG_SUPC_SFRWriteRead(NULL,0,false);
}
return result;
}