3.2.27 DIAG_TCC
The DIAG_TCC module is designed to verify the correct functionality of the Timer Controller for Control Application (TCC) through a set of C function calls.
The DIAG_TCC software test API is mapped to the following safety mechanisms:
| Function | Diagnostic Mechanism | Elapse Time (μs)~ | |
|---|---|---|---|
| DIAG_TCC_Disable() | TCC_DISABLE | POST / OnDemand | 24 |
| DIAG_TCC_DMA() | TCC_DMA | POST / OnDemand | 11.06 |
| DIAG_TCC_Enable() | TCC_ENABLE | POST / OnDemand | 17 |
| DIAG_TCC_Interrupts() |
TCC_INTERRUPTS | POST | 36.16 |
| DIAG_TCC_RedundantTimer() | TCC_REDUNDANT_TIMER | POST | 45.64 |
| DIAG_TCC_SFRReset() | SFR_RESET | POST | 83.10 |
| DIAG_TCC_SFRWriteRead() | SFR_WRITE_READ | POST / OnDemand | 84.23 |
| DIAG_TCC_SyncBusy() | TCC_SYNCBUSY | POST / OnDemand | 2100 |
#define TCC_HW_LOOP_CNTR 0x10U
#define TCC_MAX_CLOCKS_DIFF 0x5U
typedef enum diag_tcc_nums {
DIAG_TCC0_NUM = 0,
DIAG_TCC1_NUM = 1,
DIAG_TCC2_NUM = 2,
DIAG_TCC_MAX
}DIAG_TCC_NUMBERS;
typedef enum diag_tcc_periphs {
DIAG_TCC0_PERIPH = 1<<DIAG_TCC0_NUM,
DIAG_TCC1_PERIPH = 1<<DIAG_TCC1_NUM,
DIAG_TCC2_PERIPH = 1<<DIAG_TCC2_NUM,
}DIAG_TCC_PERIPHS;
typedef struct {
bool ovf_set;
bool ovf_clrd;
bool cb;
}tcc_int_status;
#define DIAG_TCC_PERIPHS_CHECK_VALUE ((uint32_t)DIAG_TCC0_PERIPH | (uint32_t)DIAG_TCC1_PERIPH | (uint32_t)DIAG_TCC2_PERIPH)
extern uint32_t tcc0_cntr, tcc0_curr_cntr, tcc0_prev_cntr, tc0_cntr, tc0_curr_cntr;
extern uint32_t tc0_prev_cntr, tcc0_tc0_curr_diff, tcc0_tc0_prev_diff;
extern tcc_int_status tcc0_ints;
extern uint32_t tcc1_cntr, tcc1_curr_cntr, tcc1_prev_cntr, tc1_cntr, tc1_curr_cntr;
extern uint32_t tc1_prev_cntr, tcc1_tc1_curr_diff, tcc1_tc1_prev_diff;
extern tcc_int_status tcc1_ints;
extern uint32_t tcc2_cntr, tcc2_curr_cntr, tcc2_prev_cntr, tc2_cntr, tc2_curr_cntr;
extern uint32_t tc2_prev_cntr, tcc2_tc2_curr_diff, tcc2_tc2_prev_diff;
extern tcc_int_status tcc2_ints;
Configuring the Diagnostic
TCC Safe-Plib can be configured as illustrated to supported to support all diagnostics:

Configuring the System

Using the Diagnostic
#include "definitions.h"
DIAG_TEST_STATUS DIAG_TCC_SFRPost ( DIAG_TCC_PERIPHS tcc_periph )
{
DIAG_TEST_STATUS result;
result = DIAG_TCC_SFRReset(tcc_periph,NULL,0,false);
if( result == DIAG_TEST_PASSED )
{
result = DIAG_TCC_SFRWriteRead(tcc_periph,NULL,0,false);
}
return result;
}
DIAG_TEST_STATUS DIAG_TCC_Post ( DIAG_TCC_PERIPHS tcc_periph )
{
DIAG_TEST_STATUS result;
result = DIAG_TCC_Enable( tcc_periph );
if( result == DIAG_TEST_PASSED )
{
result = DIAG_TCC_Disable( tcc_periph );
if( result == DIAG_TEST_PASSED )
{
result = DIAG_TCC_SyncBusy( tcc_periph );
if( result == DIAG_TEST_PASSED )
{
result = DIAG_TCC_Interrupts( tcc_periph );
if( result == DIAG_TEST_PASSED )
{
result = DIAG_TCC_DMA( tcc_periph, DMAC_CHANNEL_5 ); // DMA channel must match one set up in MCC
if( result == DIAG_TEST_PASSED )
{
result = DIAG_TCC_RedundantTimer( tcc_periph );
}
}
}
}
}
return result;
}