3.2.4 DIAG_BUSSES
The DIAG_BUSSES module is designed to verify the correct functionality of the Busses through a set of C function calls.
The DIAG_BUSSES software test API is mapped to the following safety mechanisms:
| Function | Diagnostic Mechanism | Use Case | Elapsed Time (μs)~ |
|---|---|---|---|
| DIAG_BUSSES_Fault() | EXCEPTION_HANDLER | POST | 3.18 |
#define MAGIC_HARD_FAULT_NUMBER1 0x12345678U
#define MAGIC_HARD_FAULT_NUMBER2 0x87654321UException Handling
Busses diagnostic related exception code is added in stl_exception.c file.
Note: If System integrator is using their own exception handler, an exception handler needs to be registered in vector table.
The following code should be place in the handler:
if(busfault == MAGIC_HARD_FAULT_NUMBER2)
{
busfault = MAGIC_HARD_FAULT_NUMBER1;
NVIC_SystemReset(); /* do a software reset */
}
Configuring the Diagnostic
DIAG_BUSSES does not require additional configuration.
Using the Diagnostic
#include "definitions.h"
DIAG_TEST_STATUS DIAG_BUSSES_Example()
{
DIAG_TEST_STATUS ret_value = DIAG_TEST_NOT_EXECUTED;
ret_value = DIAG_TEST_FAILED;
if (DIAG_TEST_PASSED == DIAG_BUSSES_Fault(DIAG_ADC0))
{
ret_value = DIAG_TEST_PASSED;
}
return ret_value;
}