9.10.4 Configuring FlashROM Settings in FlashPro®

To configure the FlashROM settings:

  1. From the Configuration menu, choose Load Programming File (PDB).
  2. Select the PDB file and click Open, this loads the programming file.
  3. From the Configuration menu, choose PDB Configuration. The Programming File Generator appears.
  4. Check the FlashROM checkbox and click Browse to load a FlashROM configuration file. Click Next. This brings up the FlashROM Settings dialog box (see figure below).
    Figure 9-124. FlashROM Settings Dialog Box
    ???
  5. Select the FlashROM memory page that you want to program.
  6. Enter the data value for the configured regions.
  7. If you selected the region with a Read From File, specify the file location.
  8. If you selected the Auto Increment region, specify the Start and Max values.
  9. Enter the number of devices you want to program.
  10. Click the Target Programmer button. The Select Programmer Type dialog box appears.
  11. Click Finish. FlashPoint generates your programming file.
Note: You cannot change the FlashROM region configuration from FlashPoint. You can only change the configuration from the FlashROM core generator.