9.10.1 Configuring Security, FlashROM and Embedded Flash Memory Settings in FlashPro®

  1. From the Configuration menu, choose Load Programming File (PDB).
  2. Select the PDB file and click Open, this loads the programming file.
  3. From the Configuration menu, choose PDB Configuration. The Programming File Generator appears.
    Figure 9-119. Programming File Generator
    ???
  4. Select the Silicon feature(s) you want to program:
  5. Check the Programming previously secured device(s) box if you are reprogramming a device that has been secured.

    Because the IGLOO®, ProASIC3, SmartFusion® and Fusion families enable you to program the Security Settings separately from the FPGA Array and/or FlashROM, you must indicate if the Security Settings were previously programmed into the target device. This requirement also applies when you generate programming files for reprogramming.

  6. Enter the Silicon signature (0-8 HEX characters).
  7. Click Next.